Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Will this work with all serializers

Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UH949-Q1,

Does the DS90UB954-Q1 work with all serializer, for example, the DS90UH949-Q1?

  • Hello,
    The 954 is an ADAS deserializer part so it is designed to work with the ADAS serializers such as 953, 913A, 933.
    With the 953 it can work in the CSI-2 mode with full features available. The 954 is also backwards compatible to the previous generation FPD-Link serializer parts such as the 913A and 933 in the RAW modes, but with basic functionality.
    Please refer to the DS90UB954 datasheet for details.