Part Number: TCA6424A
Other Parts Discussed in Thread: TCA6424
During the time between device reset and device programming, the TCA6424A ports are configured as inputs. In some applications, the output load could be a resistor and a series diode (as in an optocoupler LED). The leakage current of this combination could be such that the Vil of the TCA6424 may or may not be met thus causing the potential for high leakage on the port drivers (Vcc to GND) or perhaps oscillation.
The question is - is there any potential for damage to the device during the time between power on and when the ports are subsequently programmed as outputs? The time may be as long as, say 30sec for example but we'd also like to know if the state were held indefinitely, would any damage occur.
Figure 29 of the April 2014 revision indicates that resistors are required if the input pins are floating. If this is the case, then because of the default configuration, wouldn't resistors (or equivalent loads) always be required since there is always a time when the ports are configured as input after power-up?
Please advise!