This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1046A-DCI: DFP_RXDET_INTERVAL

Guru 29720 points

Part Number: TUSB1046A-DCI

Hi Team,

I found the following red part is inconsistent.
Which is the default value "00" or "01"?



Best Regards,
Yaita / Japan disty