Part Number: ISO1176T
Other Parts Discussed in Thread: , ISO3086T
Hi Experts,
When I use two ISO1176TEVM to test transmit and receive.
There is 2ns delay with 2 meters cable connection.
If I use 25 meters cable to connect with two EVM, there is no signal in receiver.
What is the longest cable length I should use for two ISO1176T/ISO3086T EVM to test ?
Thanks a lot.