Part Number: ISO1176
Hello.
A 54Ω resistor is used in the test environment of the data sheet characteristics.
In the case of 100Ω line impedance, how will "tpLH, tpHL" change?
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1176
Hello.
A 54Ω resistor is used in the test environment of the data sheet characteristics.
In the case of 100Ω line impedance, how will "tpLH, tpHL" change?
Regards,
Dice-K
Hi Dice-K,
I tried this in the lab and have confirmed the results with design.
The resistor will affect VOD and hence rise time will be the main factor here. Typical rise time is 3ns with a 54 ohm resistor. VOD would increase by roughly 1.3x for 100 ohms.
1.3 x 1.5ns = 1.95ns
This is an increase in about 450ns from the 54 ohm case. So we would not expect propagation delay to increase by more than 500ps.
500ps is a quite small change so it can be lost in the noise in a scope shot (this seems the case in my scope shots). Nonetheless I have included them for your reference. Measurements are in the bottom banner.
ISO1176 with 54 Ohm resistor:
ISO1176 with 100 Ohm resistor:
Please let me know if I've answered your question or need me to clarify anything!
Best regards,
Dan
Hello Dan,
Thank you for your reply.
I have a question about your answer.
I understand that "tr" and "tf" will be 1.3 times from your answer.
Typical "tr" and "tf" are 3ns with a 54 ohm resistor.
Will not the calculation be like this?
1.3 x 3.0ns = 3.9ns
This is an increase in about 0.9ns from the 54 ohm case.
Best regards,
Dice-K