Part Number: DP83630
Other Parts Discussed in Thread: DP83640
Hi Team,
Please allow me to ask you general questions about DP83630 and IEEE 1588.
I believe DP83630 reference clock is 25MHz or 50MHz from X1 pin.
1). The device monitors PTP packets and when it receives PTP, does DP83630 operates with the clock generated based on PTP data ?
2). What does "IEEE 1588 Clock" mean in the datasheet Figure 6-1 ? Is this clock frequency output described in "6.1.1.1.1 IEEE 1588 Clock Output" ?
3) Is the required pin connection between DP83630 and CPU would be the followings ? Please let me know if anything would be wrong.
- RMII/MII
- SMI
- GPIOx for Events and Triggers
- IEEE 1588 Clock Output (Pin# 24) for CPU to synchronize with DP83630 ?
Best Regards,
Kawai