Part Number: TUSB522P
Dear all,
For TUSB522P, I have following questions:
1. For the RX1P/1N , TX1P/1N, and RX2P/2N, TX2P/2N, they are separate pairs and can be set independently, the function of the two sets channels is also the same, am I right? in real application, those two sets can be used from either from host to receptacle or from receptacle to host, am I right?
2. For the isolated cap used, in EVM user guide, only TX pairs add 0.1uF, for RX pairs, no cap, but in datasheet, TX and RX in host side both has cap, so when do we need and this cap?
Thanks.