Part Number: DS90UB954-Q1
Hi
we are currently using the DS90UB954-Q1 on one of our boards with input 0 (RIN0) connected to a coax connector. Input 1 (RIN1) is currently not used.
We are looking into extending our board to offer both coax and STP inputs. For this we would like to connect the currently unused RIN1 input to a STP connector. As the DS90UB954-Q1 has to be configured for coax or STP only one input can be active at the same time which is fine for us. We are using power-over-coax and will provide the same voltage over STP.
Can you confirm that this approach works? Are there any pitfalls we should consider?
Many thanks