Part Number: PCA9306
Hello,
I need some advice on something that is almost a silly question to ask.
The data sheet on the PCA9306 refers only to the master being on the VREF1 side and the slave on the VREF2 side.
However, because the master is 3.3v and can go as high as 4.6v and the slave is 1.8v exact, I feel it would be best to let VREF1 handle the slave and VREF2 handle the master.
Is there any concern in doing this? - nothing I see implies there is, but just checking in case..
The ONLY thing I could see is that VREF2 requires a 200Kohm resistor which controls the current draw of the device, however in my intended application (having the slave on the other side) would the current draw be limited properly as well?
Thanks in advance for your help!
Regards,
Mark