Part Number: TCA9617B
Other Parts Discussed in Thread: TCA9517,
Hi Team,
Can I use the same voltage if VCCB and VCCA are between 2.2 V and 5.5 V?
Best Regards,
Kenji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
EDIT: please see my next reply
Hey Kenji-san,
Unfortunately this device does not support VccA=VccB. Are you choosing this device because it supports 1MHz frequency? If you don't need this supported frequency then we do have other buffers that do support VccA=VccB at 400kHz. (TCA9517 and TCA980x)
Thanks,
-Bobby
Hi Quote-san,
Thank you for answering.
Recommended operation of VCCA The MAX regulation is written in the data sheet with VCCB.
Although it can be understood that VCCA = VCCB does not matter, is that idea the wrong thing?
If VCCA <VCCB is correct, what is the voltage difference required? (For example, 1 V? 0.1V?)
Best Regards,
Kenji