Part Number: DS90UB953-Q1
Dear TI support team,
I am currently working with the following hardware setup:
An image sensor with MIPI CSI-2 interface, 4 lanes, 800Mbps/lane
connected to DS90UB953TRHBTQ1
connected to DS90UB954TRGZRQ1 via differential connection / STP cable
connected to a NXP i.MX6Q MIPI CSI-2, 4 lanes, 800Mbps/lane
The image sensor streams monochrome images at ~24fps, 640x480px in MIPI RAW12 format. The image shows a noise/corruption pattern in area px585/0 to 630/480. A screenshot is available here: http://upload.bluetechnix.at/file/0r96rah009seb3x/mipibridge.jpg
The hardware is based on the DS90UB953-Q1EVM reference schematic. The serializer is running in synchronous mode.
What could be the source of this pattern? Error registers show no errors and pattern generator image seems ok.
Thank you,
MK