Part Number: PCA9306
Hi,
This is regarding the Pullup resistor connected between EN pin and supply. From datasheet, I understand that the gate of the transistors is controlled by the voltage on the EN pin. There is no mention on the Current flowing into the EN Pin.
In datasheet, Figure 7. the value of this resistance is 200k Ohms. Is there any min and max limit for the resistance that can be used ? If so please provide the range.
Thanks,
Praveen