Part Number: DS64BR111
The datasheet DS64BR111 SNLS343C revised April 2013 is missing a bit in a register.
Page 28 Address 0x23 register: BR111 CH A VOD is missing bit 5. I assume bit 5 falls with Reserved 7:6, but would like this confirmed.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS64BR111
The datasheet DS64BR111 SNLS343C revised April 2013 is missing a bit in a register.
Page 28 Address 0x23 register: BR111 CH A VOD is missing bit 5. I assume bit 5 falls with Reserved 7:6, but would like this confirmed.
Hi Richard,
You are correct. Bit 5 in Reg 0x23 is a reserved bit and is set by default to 0'b.
Thanks,
Michael