This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UR910-Q1: Can NOT receive any signal

Part Number: DS90UR910-Q1
Other Parts Discussed in Thread: DS90UR905Q-Q1, , ALP

Hi,

I'm using DS90UR905Q-Q1 as serializer and DS90UR910-Q1 as deserializer. The serializer board is made by gerber file from TI's website and the deserializer board is DS90UR910QEVM.

After connected the serializer and deserializer, the PASS and LOCK on DS90UR910-Q1 are always low and there is no any signal on the output. Now I do NOT configure any register, because it says that it is optional in the DS90UR910QEVM guide.

I MUST configue the register in DS90UR905Q-Q1 and DS90UR910-Q1. Is that right? Or is that optional?

If the register must be configured, what registers must be configured?

Thanks.

Kevin Xiong