Part Number: UCC21520
Hi all,
I'm using the UCC21520 to drive the gates of two IGBT. These IGBT's switch a high voltage capacitor to a solenoid. However, the module breaks after driving the gate a few times, even when there is no voltage on the source of the IGBT. I'm using 5V for the VCC and 18V for the VDD.
When the driving breaks, only one of the two channels breaks. The other channel can still be used until it also ends up breaking. When driving a broken channel, the UCC tries to get the gate to 18V, but the internal pull-down MOS also seems to get shorted. The voltage on the output pin and the 18V drops, until it goes into under voltage lockout.
The input signal goes through an isolator, the ISO7241cqdwrq1. The input of this isolator is controlled with a button. Could a bouncing input signal from this button be a problem?
I've attached the schematic and the layout on the PCB. I highlighted the paths from the isolator to the driver and the output of the driver to the gate of the IGBT's. I believe these traces should be short enough not to cause any issues.
Thanks for your time. If you have any questions, I'll try to respond as soon as I can.