Part Number: DS90UB914A-Q1
Hi team,
Our customer is using 913A and 914A with 10bit mode.
They assume that 914's MODE pin short-circuits to GND due to some abnormality and is set to 12 bit mode.
When correct 10 bit data is sent from 913A, how will 914A handle this data?
In their experiments, there seem to be cases in which the 914A outputs data or does not output .
They hope that the 914A can judge that the data format is incorrect.
Otherwise, does the 914A handle the lower 10 bits of 12 bits and output data and sync?
Or will 914A sort 12bits as completely random data and output?
Best regards,
Tomoaki Yoshida