Part Number: TPS65982
Other Parts Discussed in Thread: TPS65981, TPS65987
Hello E2E,
A customer of mine is looking to use the TPS65982 and they have some questions:
- Linux drivers - what kernels are supported?
- Application currently is using Linux Kernel 4.04 – preference to not upgrade Kernel to risk delaying time to market
- Is power path supported (USB-C delivers power to the device when connected and not the battery)? If not, what part would you recommend?
- How is the device programmed in a production setting?
- Are drivers required? Does TI have anything? (there is no time in the project to do any driver development)
- How to do SW and HW setup for field programmability of the TPS firmware?
- Use cases are
- System is powered down on battery, when PD is plugged in the TPS needs to negotiate the power sinking configuration (e.g. 15V 2A) so the battery charger can come on and so the system optionally could be powered up
- Same but no battery, PD needs to autonegotiate and switch on the 15V from the PD
- Power and data to a USB 3.0 type C device like a flash drive
- Power and data to a USB 2.0 type C device (don’t know what this device is yet)
-
it needs to be both an upstream and downstream data port.
Also to include one additional question up front – if the CPU SOM has Linux 4.04 support for USB 3.0, is everything else in the TPS firmware? i.e. no Linux support or drivers for the PD and data negotiations, just programming / configuring the TPS firmware and it handles that?
Finally, as a generic question, what you suggest between the TPS65982 and TPS65981?
Thanks!
Russell