Part Number: TPS65982
Hi,
My customer has the following question:
We have a design where the VBUS supply to PD controller cannot be turned off without shutting down the entire device. And if VBUS is on, the external devices connected to the Type C port stay powered. So we tried to disable the power by disabling port. One way to do it is by writing the bits b'111 to the bits 2:0 of the register 0x28. This seems to work fine on the firmware images based on the 1.11.5 firmware, but fails (does nothing) on 1.11.0.
Right now we have a certain number of devices in customers' hands, without an easy way to update them - all using 1.11.0 firmware
Is there a way to disable VBUS supply (by any means) on 1.11.0 firmware builds?
Thanks,
Chuchen