Part Number: SN65DPHY440SS
Team,
I am supporting a customer that is using a MIPI-DSI interface to drive an LCD display (sink) over a 22" custom cable. They are running the display from an Intel processor (source).
They are currently using 3 of the MIPI diff pairs (2 data + CLK) (clock is ~290MHz).
As I understand, the display is intermittently going dark (not sure if caused by software or hardware yet but would like to explore hardware setup troubleshooting).
They don't have the equipment to measure an eye-diagram to see if the 22" length is causing them issues.
Do you have any recommendations for troubleshooting this scenario on the hardware side?
They currently don't have the SN65DPHY440SS implemented in the system, but are interested in obtaining an EVM to troubleshoot and test for a performance improvement. Any recommendations you can provide would be appreciated.
Thanks.