This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7340: Power sequence issue

Part Number: TUSB7340

Hello

                Has any 3.3V and 1.1V power sequence requirement for these two supply? or It have no power sequence concern. Another question, do we need to stable 3.3V/1.1V then plug into USB device? Or we can plug into USB device before 3.3V/1.1V supply stable and can not cause any access USB device issue. Thank you. 

BR

Patrick

  • Patrick,

    As long as GRST# is low, there should be no sequence requirement for 1.1V and 3.3V supplies.   If you plug in a device before PERST# is high and the xHCI driver is loaded, VBUS would not be enabled to the device and there is no access to the device until the power is stable.

    Regards,

    Brian