Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB422: TUSB422 VCONN power connect

Part Number: TUSB422

Hi Team

My customer ask for TUSB422 VCONN connection. They want to know if it can use battery voltage(3.4~4.4V) not use boost 5V voltage?

It is a cell phone project. I saw spec 8.2.2 mention that type-C redefine VCONN from 3.3V~5.5V, but I just want to sure if this kind of connect to battery can work fine or not.

Do you have some expenience about this?

Thanks

Bruce