Hello I am need of an image ( .bin ) file that can be used for Thunderbolt reference design called: AR LP BPD USB3_1 II REV1V2_Final
Also it will be nice to have a design tool from TI that supports TPS65983B - the only one I could find was
TPS6598x Application Customization Tool version 3.11 , but the reference intel designs doesn't even drive GPIO2 which is needed for starting up the Alpine Ridge.
Thanks,
Vasil Savov