Part Number: TPS2553
Hi all
Would you mind if we ask TPS2553?
<Question1>
We have the question TPS2553-1(Latch off type).
How much is the response time to Short-Circuit or overcurrent?(2us?)
Otherwise, if there is 2us noise insertion, will TPS2553-1 be latch off?
<Question2>
FAULT deglitch on the datasheet, does it correspond for TPS2553-1(Latch off time)?
<Question3>
We have the question TPS2553(Constant-Current type).
In case of output current 0A - 0.7A - 0A - 0.7A - 0A - 0.7A 1ms interval with current limit=0.55A or 0.45A, what kind of action does FLT pin operate?
FAULT deglitch is min 5ms. So we assume that FAULT pin keeps high(no active).
Is our recognition correct?
Kind regards,
Hirotaka Matsumoto