Part Number: DP83822H
Hi.
In Datasheet Revision C (April 2018), Pin 24 (LED_1/GPIO1), becomes a strapping pin, according to table on page 7. (This was not the case in older revisions).
The following can be found:
"This pin must have a pulldown or pullup external resistor when not used to prevent bootstrapping to MODE 2 or MODE 3."
My question:
Which bootstrap function has this pin? In the table of the strapping pin description (table 11), this pin is not described.
Also the two registers, which are storing the strapping information (0x0467 & 0x0468), are not updated in this datasheet revision with the Pin 24 strapping information.
Is Pin 24 realy a strapping Pin, or is it an issue in the Pin description?
If it is a strapping pin, what function is behind this strapping?
Best regards,
Christian