Part Number: TUSB522P
Other Parts Discussed in Thread: TUSB211, TUSB212, SN65LVPE512
Hi,
I am working on developing one IP camera with USB port. To improve video signal quality, I want to add a USB3.0 redriver.
I found TUSB522P seems suitable for my application. Since I need it to be compatible with usb2.0, does TUSB522P can do this?
Or should I add another usb2.0 redriver like TUSB211, if do so, will there be any problem with two usb redriver?
When looking the datasheet of TUSB522P, I found the gain is all under 2.5GHz condition, but theoretically USB3.0' s bandwidth is 5GHz.
Does that mean under super-speed mode, USB3.0's TX and RX only has 2.5GHz clock frequency seperately?
If have any other better recommendation, please help to give suggestion. Thank you.