Part Number: DP83640
Other Parts Discussed in Thread: DP83620
Hi everyone,
We are working on a design with the DP83649 PHY in 100BASE-FX mode and the Broadcom/Avago HFBR-5963ALZ which uses LVPECL interface.
I am a bit confused about the proper termination of the TD+/- pair. I understand the PHY transmitter is an open drain output, so it needs the 50ohm pull-ups and because the Avago transceiver is LVPECL we have to use AC-coupling and then properly bias the LVPECL side.
What has me confused is the fact that in the PHY datasheet it recommends to use 130ohm/82ohm pull-up/pull-down termination, but in the TI scaa059c app note when it explains terminations for an AC-coupled LVPECL interface it says it requires a 83/130 termination because LVPECL needs 2V common mode voltage.
Which one is right?
Regards and thanks in advance!