This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA7408: TCA7408 0x09 default state

Part Number: TCA7408


Hi, Team

In TCA7408's datasheet, page 19, 8.6 Register Table, the power up default state of REG09h is 0x00.

But on page 20, in the description of REG 09h is 11111111b".

The question is which one is the correct one?

  • Hey Harson,

    The description on page 20 is incorrect and should display 0000 0000b.

    I put this correction in our backlog list so we will make changes to the datasheet at a later point in time.

    Thanks,
    -Bobby