Part Number: DS280DF810
Dear E2E,
What is the requirement of internal eye diagram in DS280DF810?
VEO>200mV and HEO>0.44UI
my question is that is it must to meet both requirement. what if only meet one of criteria, which one is more important?
in fact, we tried a lot of setting of FIR combination in ASIC, but the internal eye of Retimer still can't meet both requirement. only pass HEO criteria.
the insertion loss is less than 35dB.
or
any tip or direction can improve the internal eye diagram?
BR,
Jason