Part Number: TPD6S300
Other Parts Discussed in Thread: TPD2S300, TPD1E05U06-Q1
We are using a FTDI FT601 controller to communicate with our USB TYPE C connector. It has the following ESD protection (taken from Data sheets)
In our design we have connected the USB 2.0 DP/DN signals to a TPD6S300 (which we also use to protect the CC lines).
1. Is the above protection provided by the FT601 chip enough that we can replace the TPD6S300 with smaller simpler TPD2S300 that will only protect the CC lines ?
2. If the above protection is not enough - is there any issues of double protection and the effect on the USB signals ?
Best regards
Shmuel