Part Number: DP83867IR
I am using DP83867IR EVM in 100Mbps MII Mode (GTX_CLK, RXD4..7 and TXD4..7 not connected). The CLKOUT pin on J8 is used as clock source for our design. RX_CLK is providing a 25MHz clock after forcing to 100MBps (disable 1000BASETFULLDUPLEX and 1000BASETHALFDUPLEX in CFG1). Link is established with 100M as expected. No data communication is possible. TX_CLK is driving '0' (tested with pull-up). Expected is a 25MHz clock output.
What could be wrong?