This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983B: Thunderbolt Questions

Part Number: TPS65983B

I have a customer who is developing a Thunderbolt 3 design with the TPS65983B. He has questions regarding the SPI interface and a bin file that he generated below:

1.  I'm working this with another engineer and he had a question too.  He put an Aardvark I2C from Totalphase on the line and he saw the I2C lines polling address 0x3F.  When he acknowledged that it quit.  Is that expected behavior?

2.  I was looking at the bin file generated by Intel when I add the TPS65983B code in.  It has pointers at 0x0 and 0xFFC like I would expect.  However there are none at 0x1000 or 0x1FFC.  Also the first set is pointing to the Region Pointer in the low header.  Is this okay or do the pointers need to be adjusted per the TPS65983 Firmware User's Guide?

Please let me know if you have any further questions for the customer.

Thanks for your help with this!

Richard Elmquist