Part Number: TLK2501
Hi,
I didn't get it properly from the data-sheet but hope to have found the solution to my problem:
I got 14 digital signals at 125MBit/s.
All the signals are a different source, not related to each other.
I want to transmit those 14 signals across an optical link and split them again to 14 parallel data-ports.
But I do not yet see how to initialize and synchronize the TLK2501.
The synchronisation between the two TLK2501 is happening by the comma-detection?
Is this happening automatically?
Or do I have to wait till the TLK2501s are synced and then switch ON my data-inputs?
Or do I have to provide the comma-patterns on the inputs?
I don't have a FPGA and don't have the option to generate any specific parallel pattern.
In another post I've read that only some of the pins need to be toggled.
Sadly I didn't get how that needs to be done.
If you could provide some information where I can get more details about that I`d be really glad.
Kind regards,
Robert