Part Number: TUSB321
Hi,
I am using TUSB321 in the design as UFP.
I need some information about the OUT1 and OUT 2 output signals in TUSB321.
These 2 signals are used to identify the current level detection in TUSB321. But, I want to know the time delay required to generate the ouptut signals on OUT1 / OUT2 pins after the CC1/CC2 detects the current level.
From my designs, I have noted this valuse as 180ms( CC pins detection to OUT1/OUT2 generation).