Part Number: SN65HVD23
Hi,
I wanted to know the current required(max current consumption) for the below mentioned parts
| SN65HVD233 |
| SN65HVD234 |
| SN65HVD235 |
Regards,
Karthik
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Karthik,
The resistance load draws the most current. Assume the device generates 1.5V on a 60Ohm resistor. The current is 25mA. The device itself needs maximum 6mA, in active states. Since the data rate is low (<2Mbps), the current due to AC load is less than 1mA. Please let me know if you more questions.
Regards,
Hao
Hi Hao,
How did you come to the conclusion that I=25mA for 1.5V output @ 60ohm load , Is there any formula to calculate the supply current?
What are the protections(transients,short circuit) that are to be given on the SN65HVD234 bus lines ?
Please can you share the recommended parts for protection or can I get a reference schematic for the above part.?
Please suggest
Regards,
Karthik
Karthik,
25mA current comes by dividing 1.5V Vod by the termination resistance (60Ohm), which is drawn from the supply. The device comes with short protection. The maximum short current (Ios) is less than 250mA. For transient event protection like ESD, you can refer to this app note (http://www.ti.com/lit/ug/tidub36b/tidub36b.pdf). Please let me know if you have more questions.
Regards,
Hao