Part Number: DP83TC811R-Q1
Hi team,
I have a question.
I will use LED_0 and LED_1.
Register 0x0469 bit 6 and bit 2 have registers to set the polarity.
It is written that the default of them are strap.
When strap is pulled down, 0 is written in this field and initialized to active low.
Is this correct?
Which of these pins is internally pulled up or pulled down?
I want to use the strap by pull-down as shown on the left side of the data sheet in Figure 28, so I want to check how to set it up.
Best regards,
Tomoaki Yoshida