This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: How to configure the 954,953?

Part Number: DS90UB954-Q1

Hello,

How to configure the  954,953?For example, my camera specifications are as follows:
Resolution: 1920 X 1080;
Frame rate: 30;
Number of lanes: 2lane;
Data Format: CSI RAW 12bit;

954 configuration:
1: VDDSEL = 0 1.1V with internal LDO
2: IDX 10K pull-down Pull-up NC I2C address: 0011 000x
3:mode 78.7K pull-up 97.6K pull-down
953 configuration:
1: IDX 40.2K drop-down
2:mode pulls down 4780 NON-Synchronous mode

The camera MIPI signal has been output, but there is no MIPI signal output on the 954 side. Please help.