This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986: TPS65986 20V plus DP support for both source and sink

Part Number: TPS65986

I need to update my TPS65986 EVMs (with DP breakout board) to support 20V source and DP source (source side board) as well as a 20V sink and DP sink (sink board).  Can someone send me the updated config file along with a brief tutorial on updating the EVM?

Thanks,

Dan 

  • Hi Dan,

    Please make sure you are using the latest version of our configuration tool from TI.com. For the DP Source/20V source board, you could start with the TPS65986 DFP template. With that you can change the Source Capabilities register and make sure there is a 20V source PDO available. For the 20V Sink and DP sink board, you could start with the TPS65986 UFP template and make sure you have a 20V Sink PDO in the Sink Capabilities register.

    When you open the App Customization Tool you can filter through our templates when clicking Project --> New project.

    If this answers your question, PLEASE select  This resolved my issue

    Thank you,

    Eric