Part Number: HD3SS3220
Other Parts Discussed in Thread: TUSB320
In the following thread :-

Since the VDD5 for the HD3SS3220 I am powering from VBUS it was recommended that I use a diode similar to the implementation shown for the TUSB320 UFP configuration
1. What is the purpose of this diode for the HD3SS3220 ?
2. As far as I understand the VBUS range is 4.75V - 5.5V. If VBUS drops close to 4.75 won't the diode drop the VDD5 for the HD3SS3220 to below 4.5V min ?
Thank you
Shmuel