This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: FPD3_PCLK in RAW mode

Guru 29720 points

Part Number: DS90UB954-Q1

Hi Team,

I understood the following according to Table 4.
- RAW 10-bit mode: FPD3_PCLK = PCLK_Freq. /2
- RAW 12-bit HF mode: FPD3_PCLK = PCLK_Freq. x 2/3
-------------------------------------------------------

-------------------------------------------------------

On the other hand, the following shows "FPD3_PCLK=100MHz"(red line) although input PCLK range is up to 100MHz.
-------------------------------------------------------

-------------------------------------------------------

I believe "FPD3_PCLK=100MHz"(red line) is typo and "PCLK_Freq=100MHz" is the correct.
Is my understanding correct?

Best Regards,
Yaita / Japan disty