Part Number: SN65LVDM176
Other Parts Discussed in Thread: ISO7821LL, ISO7710, SN6501
I inherited a design using SN65LVDM176 half-duplex LVDS transceiver. Speeds in application are fairly pedestrian (up to 25mbps). The LVDS pair is sent between 2 separate boards, each possibly using different power supplies. Only the LVDS data lines might be common between the boards. The transceivers can be damaged on a hotplug (and/or pull) event as well as if one board is not connected to a power supply (not grounded) but receiving some signal on LVDS lines from a powered board. I'm investigating solutions to this issue and thinking that isolating the transceiver from the incoming LVDS signaling to prevent current from entering the transceiver until a ground and power has been established might be a solution to the issues observed.
I understand that hotplug/pull could possibly be alleviated by forcing ground to be connected first in a mechanical solution, but the connector type being used doesn't have this feature and may be out of the question for this design. This also wouldn't solve the issue with one board ungrounded but receiving LVDS signals.
- Is isolation a solution to the problems described?
- I haven't seen any specific isolated half-duplex LVDS transceiver reference designs. Are there any examples available?
- Recommendation on isolation part that could be paired with SN65LVDM176DR or one of the newer M-LVDS compliant transceivers?
Any assistance and advice would be greatly appreciated.