This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65C1168E: specification for SN65C1168E

Part Number: SN65C1168E

Hi,

Kindly provide below details for Part#  SN65C1168E

  1. Maximum Cable length SN65C1168E can operate.
  2. How many SN65C1168E nodes will be connected on RS485 bus.

  • Yash,

    The SN65C1168E is guaranteed to operate in accordance with the TIA/EIA-422-B  standard. The figure below provides a general to to cable length vs speed that the RS 422 devices can handle. The device can output a a recommended maximum of 20mA and -20mA on the bus lines. The maximum number of nodes being driven has to comply with these current thresholds. 

    TIA/EIA-422-B  standard

    -Lucas