This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: CSI-2 output when input CSI_CLK frequency with 953 is lower than output with 954

Part Number: DS90UB954-Q1


Hi team,

I will use the camera module integrate 953, its CSI_CLK is 184MHz and it use 4-lane of CSI-2.

I will use 954 to set 400MHz CSI_CLK and 2-lane.

Will CSI output of 954 is in intermittent operation?

Best regards,

Tomoaki Yoshida