Part Number: SN65DSI85-Q1
Other Parts Discussed in Thread: SN65DSI84, SN65DSI85
I've been using the SN65DSI84 in Flatlink Output Data (Format 1) single link 24bpp mode to drive a single panel. Now I'd like to drive two panels. Can the SN65DSI85 drive two separate paths where A and B input and output are isolated from one another? In other words can I drive one image into DSI A and get a single output on LVDS A, then a different image on channel B? Or do I need to use two seperate parts for that?
Would it be possible if I wanted to drive the same image to panel A and panel B?
Thank you