Part Number: DS90UB921-Q1
The DS90UB921 datasheet 8.3.2 Page 44 states that the link capacitors should be the same at both the serialiser and the desierialiser and 0.33uF and 0.15uF are recommended elsewhere in the datasheet
but the DS90UB940 datasheet 9.2.1 states that there is a DC-balanced decoding scheme - recommend 33nF and 15nF which are an 10 times smaller than this.
What are the requirements for the DC-balancing scheme to work? Should we use 33nF and 15nF at both ends for the UB921/UB940 combo?