Hello all,
I think about using the DS110DF111 for retiming the Ethernet signals.
In a kind of power save mode, I want to monitor the LOS/INT# signal to detect a valid signal at the input in order to wake up parts of my hardware.
In this power saving mode there are no signals at the inputs INA and INB, and I have a low budget for power consumption in this state.
So I have two question regarding this:
1) What is the power consumption value of the DS110DF111, if there are no signals at the inputs of both channels ?
2) Do I need to supply the reference clock (at this stage) for the signal detection function (driving the LOS/INT# signal) ?
Many thanks,
Michael