Part Number: TUSB212
Dear E2E,
How to configure TUSB212 operated in pin strap mode?
tie SCL/CD pin to high or left floating is ok or other correct way.
BR,
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Malik,
If so, why dataheet in the section of 7.4.3 mentioned that enable signal compensation with CD pin assert high?
BR,
Jason
I2C configuration only occurs when both SDA and SCL are pulled high and is enabled only during a configuration time directly after reset. High Speed signal compensation will always be on by default in both I2C and Non I2C mode. Signal compensation settings can be controlled through the EQ pin (See Table 3 in TUSB212 datasheet).