Part Number: TUSB544
Other Parts Discussed in Thread: SN65LVPE512, TUSB522P
Hello!I use this IC of TUSB544I as the USB3.0 Redriver to realize the Redriver function of the two USB3.0, and the specific lines are attached.
Test method: using the OK USB3.0 usb drive (which works normally on Dell desktop), the usb flash disk cannot be identified;Use USB2.0 usb flash drive to catch usb flash drive.
Configuration: I2C_EN/dir1-name/DIR0 / CTL1 / CTL0 / FLIP = 011110.
Please help to analyze it, thank you!