Part Number: PCI2050B
Hello E2E,
I am posting on behalf of a customer.
I have been tasked with looking at the PCI2050B as a replacement for the PCI2050 in one of our products.
I have read through the "comparing PCI2050B to PCI2050" document (SLAA199) but I just wanted to get some clarification and ask some questions.
I think I read that the main difference is with pin 125 and and pin 102 and we would need to have a pull down on these pins in order to maintain our 33MHz operation on the bus, is that correct?
Is it okay to leave pin 153 unconnected? (It is Not Connected in our application).
One of the other things I saw was this note for P_Vccp and S_Vccp about recommending to power them up before Vcc:
We currently have those pins all connected to the same 3.3VDC. Will this be an issue?
Do you recommend any additional capacitance be added to the Vcc pins for the 2050B part?
Are there any other gotchas that aren't obvious in the datasheet?
Thanks!
Regards,
Russell