Part Number: TCA9548A
1) I would like to confirm if each channel SD0-7/SC0-7 can operate at different modes (ie SD0/SC0 @ FAST kHz Normal 100kHz) or is the speed related to the speed of the master? Therefore, if SDA/SCL is 400kHz, then all channels SD0-7/SC0-7 would be at 400kHz?
2) Also, I saw a previous post regarding Vpass. It appears that it I have any bus at 1.8V, then my VCC needs to be <=3V. However, SDA/SCL can operate at V_high=0.7*VCC-6.0V.
This means that I can have
a) A channel at 1.8V
b) VCC=2.5V
c) SDA/SCL=3.3V
Did I miss anything here?
Thank you!