Part Number: DS110RT410
Other Parts Discussed in Thread: DS110DF410EVM
I want to lock to a 1.25g signal ,here are my register settings,I do it strictly to the mannual.
<0xff,0x04> //select cha0 register
<0x2f,0x06>//vco coarse range Ethernet
<0x36,0x31>//ref mode3
<0x60,0x00>,<0x61,0xb2>,<0x62,0x90>,<0x63,0xb3>,<0x64,0xff> //Nppm and ppm tolerance
<0x0a,0x1c>//
<0x0a,0x10>//reset cdr
but the cdr status 0x2 is always zero no matter what speed signal I put
Q1:why that happen,Did I miss something important to set?
Q2:I change 0x2f to 0x26 which sets the vco frequency to 10Gbps ,and I override the vco divider 0x18 to 0x30 which means 8; and i get the status to become 0xc4,but still not lock,why?
the situation really drives me mad,really appreciate your help, :-)